1.3.4.1.7 MAC_PLC_SetRequestSync Function
C
MAC_STATUS MAC_PLC_SetRequestSync
(
MAC_PLC_PIB_ATTRIBUTE attribute,
uint16_t index,
const MAC_PIB_VALUE *pibValue
);
Summary
The MAC_PLC_SetRequestSync primitive sets the value of an attribute in the MAC PLC layer Parameter Information Base (PIB).
Description
SetRequestSync primitive is used to set the value of a PIB. Sync suffix indicates that result of set operation is provided upon function call return, in the return status code.
Precondition
MAC_PLC_Init routine must have been called before.
Parameters
| Param | Description |
|---|---|
| attribute | Identifier of the Attribute to provide value. See MAC_PLC_PIB_ATTRIBUTE. |
| index | Index of element in case Attribute is a table. Otherwise index must be set to '0'. |
| pibValue | Pointer to MAC_PIB_VALUE object where value is contained. |
Returns
Result of set operation as a MAC_STATUS code.
Example
MAC_STATUS status;
const MAC_PIB_VALUE value = {
.length = 1,
.value = 6
};
status = MAC_PLC_SetRequestSync(MAC_PIB_MAX_FRAME_RETRIES, 0, &value);
if (status == MAC_STATUS_SUCCESS)
{
// PIB correctly set
}
Remarks
None.