1.3.4.1.9 MAC_PLC_PIB_ATTRIBUTE Enum
C
typedef enum
{
MAC_PIB_MAX_BE = 0x00000047,
MAC_PIB_BSN = 0x00000049,
MAC_PIB_DSN = 0x0000004C,
MAC_PIB_MAX_CSMA_BACKOFFS = 0x0000004E,
MAC_PIB_MIN_BE = 0x0000004F,
MAC_PIB_MAX_FRAME_RETRIES = 0x00000059,
MAC_PIB_TIMESTAMP_SUPPORTED = 0x0000005C,
MAC_PIB_SECURITY_ENABLED = 0x0000005D,
MAC_PIB_FRAME_COUNTER = 0x00000077,
MAC_PIB_DUPLICATE_DETECTION_TTL = 0x00000078,
MAC_PIB_HIGH_PRIORITY_WINDOW_SIZE = 0x00000100,
MAC_PIB_TX_DATA_PACKET_COUNT = 0x00000101,
MAC_PIB_RX_DATA_PACKET_COUNT = 0x00000102,
MAC_PIB_TX_CMD_PACKET_COUNT = 0x00000103,
MAC_PIB_RX_CMD_PACKET_COUNT = 0x00000104,
MAC_PIB_CSMA_FAIL_COUNT = 0x00000105,
MAC_PIB_CSMA_NO_ACK_COUNT = 0x00000106,
MAC_PIB_RX_DATA_BROADCAST_COUNT = 0x00000107,
MAC_PIB_TX_DATA_BROADCAST_COUNT = 0x00000108,
MAC_PIB_BAD_CRC_COUNT = 0x00000109,
MAC_PIB_NEIGHBOUR_TABLE = 0x0000010A,
MAC_PIB_FREQ_NOTCHING = 0x0000010B,
MAC_PIB_CSMA_FAIRNESS_LIMIT = 0x0000010C,
MAC_PIB_TMR_TTL = 0x0000010D,
MAC_PIB_TONE_MASK = 0x00000110,
MAC_PIB_BEACON_RANDOMIZATION_WINDOW_LENGTH = 0x00000111,
MAC_PIB_A = 0x00000112,
MAC_PIB_K = 0x00000113,
MAC_PIB_MIN_CW_ATTEMPTS = 0x00000114,
MAC_PIB_CENELEC_LEGACY_MODE = 0x00000115,
MAC_PIB_FCC_LEGACY_MODE = 0x00000116,
MAC_PIB_BROADCAST_MAX_CW_ENABLE = 0x0000011E,
MAC_PIB_TRANSMIT_ATTEN = 0x0000011F,
MAC_PIB_POS_TABLE = 0x00000120,
MAC_PIB_POS_RECENT_ENTRY_THRESHOLD = 0x00000121,
MAC_PIB_POS_RECENT_ENTRIES = 0x00000122,
MAC_PIB_PLC_DISABLE = 0x00000123,
MAC_PIB_PREAMBLE_LENGTH = 0x00000124,
// manufacturer specific
// provides access to device table
MAC_PIB_MANUF_DEVICE_TABLE = 0x08000000,
// provides access to neighbour table by short address (transmitted as index)
MAC_PIB_MANUF_NEIGHBOUR_TABLE_ELEMENT = 0x08000002,
// returns the maximum number of tones used by the band
MAC_PIB_MANUF_BAND_INFORMATION = 0x08000003,
// Short address of the coordinator.
MAC_PIB_MANUF_COORD_SHORT_ADDRESS = 0x08000004,
// Maximal payload supported by MAC.
MAC_PIB_MANUF_MAX_MAC_PAYLOAD_SIZE = 0x08000005,
// Resets the device table upon a GMK activation.
MAC_PIB_MANUF_SECURITY_RESET = 0x08000006,
// Forces Modulation Scheme in every transmitted frame
// 0 - Not forced, 1 - Force Differential, 2 - Force Coherent
MAC_PIB_MANUF_FORCED_MOD_SCHEME = 0x08000007,
// Forces Modulation Type in every transmitted frame
// 0 - Not forced, 1 - Force BPSK_ROBO, 2 - Force BPSK, 3 - Force QPSK, 4 - Force 8PSK
MAC_PIB_MANUF_FORCED_MOD_TYPE = 0x08000008,
// Forces ToneMap in every transmitted frame
// {0} - Not forced, other value will be used as tonemap
MAC_PIB_MANUF_FORCED_TONEMAP = 0x08000009,
// Forces Modulation Scheme bit in Tone Map Response
// 0 - Not forced, 1 - Force Differential, 2 - Force Coherent
MAC_PIB_MANUF_FORCED_MOD_SCHEME_ON_TMRESPONSE = 0x0800000A,
// Forces Modulation Type bits in Tone Map Response
// 0 - Not forced, 1 - Force BPSK_ROBO, 2 - Force BPSK, 3 - Force QPSK, 4 - Force 8PSK
MAC_PIB_MANUF_FORCED_MOD_TYPE_ON_TMRESPONSE = 0x0800000B,
// Forces ToneMap field Tone Map Response
// {0} - Not forced, other value will be used as tonemap field
MAC_PIB_MANUF_FORCED_TONEMAP_ON_TMRESPONSE = 0x0800000C,
// Gets Modulation Scheme of last received frame
MAC_PIB_MANUF_LAST_RX_MOD_SCHEME = 0x0800000D,
// Gets Modulation Scheme of last received frame
MAC_PIB_MANUF_LAST_RX_MOD_TYPE = 0x0800000E,
// Indicates whether an LBP frame for other destination has been received
MAC_PIB_MANUF_LBP_FRAME_RECEIVED = 0x0800000F,
// Indicates whether an LBP frame for other destination has been received
MAC_PIB_MANUF_LNG_FRAME_RECEIVED = 0x08000010,
// Indicates whether an Beacon frame from other nodes has been received
MAC_PIB_MANUF_BCN_FRAME_RECEIVED = 0x08000011,
// Gets number of valid elements in the Neighbour Table
MAC_PIB_MANUF_NEIGHBOUR_TABLE_COUNT = 0x08000012,
// Gets number of discarded packets due to Other Destination
MAC_PIB_MANUF_RX_OTHER_DESTINATION_COUNT = 0x08000013,
// Gets number of discarded packets due to Invalid Frame Lenght
MAC_PIB_MANUF_RX_INVALID_FRAME_LENGTH_COUNT = 0x08000014,
// Gets number of discarded packets due to MAC Repetition
MAC_PIB_MANUF_RX_MAC_REPETITION_COUNT = 0x08000015,
// Gets number of discarded packets due to Wrong Addressing Mode
MAC_PIB_MANUF_RX_WRONG_ADDR_MODE_COUNT = 0x08000016,
// Gets number of discarded packets due to Unsupported Security
MAC_PIB_MANUF_RX_UNSUPPORTED_SECURITY_COUNT = 0x08000017,
// Gets number of discarded packets due to Wrong Key Id
MAC_PIB_MANUF_RX_WRONG_KEY_ID_COUNT = 0x08000018,
// Gets number of discarded packets due to Invalid Key
MAC_PIB_MANUF_RX_INVALID_KEY_COUNT = 0x08000019,
// Gets number of discarded packets due to Wrong Frame Counter
MAC_PIB_MANUF_RX_WRONG_FC_COUNT = 0x0800001A,
// Gets number of discarded packets due to Decryption Error
MAC_PIB_MANUF_RX_DECRYPTION_ERROR_COUNT = 0x0800001B,
// Gets number of discarded packets due to Segment Decode Error
MAC_PIB_MANUF_RX_SEGMENT_DECODE_ERROR_COUNT = 0x0800001C,
// Enables MAC Sniffer
MAC_PIB_MANUF_ENABLE_MAC_SNIFFER = 0x0800001D,
// Gets number of valid elements in the POS Table
MAC_PIB_MANUF_POS_TABLE_COUNT = 0x0800001E,
// Gets or Sets number of retires left before forcing ROBO mode
MAC_PIB_MANUF_RETRIES_LEFT_TO_FORCE_ROBO = 0x0800001F,
// Gets internal MAC version
MAC_PIB_MANUF_MAC_INTERNAL_VERSION = 0x08000021,
// Gets internal MAC RT version
MAC_PIB_MANUF_MAC_RT_INTERNAL_VERSION = 0x08000022,
// Resets MAC statistics
MAC_PIB_MANUF_RESET_MAC_STATS = 0x08000023,
// Enable/Disable Sleep Mode
MAC_PIB_MANUF_MAC_RT_SLEEP_MODE = 0x08000024,
// Set PLC Debug Mode
MAC_PIB_MANUF_MAC_RT_DEBUG_SET = 0x08000025,
// Read PLC Debug Information
MAC_PIB_MANUF_MAC_RT_DEBUG_READ = 0x08000026,
// Provides access to POS table by short address (referenced as index)
MAC_PIB_MANUF_POS_TABLE_ELEMENT = 0x08000027,
// Minimum LQI to consider a neighbour for Trickle
MAC_PIB_MANUF_TRICKLE_MIN_LQI = 0x08000028,
// LQI for a given neighbour, which short address will be indicated by index. 8 bits.
MAC_PIB_MANUF_NEIGHBOUR_LQI = 0x08000029,
// Best LQI found in neighbour table. 8 bits.
MAC_PIB_MANUF_BEST_LQI = 0x0800002A,
// PLC Interface availability. 8 bits (bool).
MAC_PIB_MANUF_PLC_IFACE_AVAILABLE = 0x0800002B,
// Last PLC frame duration in ms. 16 bits.
MAC_PIB_MANUF_LAST_FRAME_DURATION_PLC = 0x0800002C,
// Resets TMR TTL for the Short Address contained in Index. 8 bits.
MAC_PIB_MANUF_RESET_TMR_TTL = 0x0800002E,
// Gets or sets a parameter in Phy layer. Index will be used to contain PHY parameter ID.
// Check 'enum EPhyParam' in MacRtMib.h for available Phy parameter IDs
MAC_PIB_MANUF_PHY_PARAM = 0x08000020
} MAC_PLC_PIB_ATTRIBUTE;
Summary
Lists the available objects in the MAC PLC Parameter Information Base (PIB).
Description
MAC PIB is a collection of objects that can be read/written in order to retrieve information and/or configure the MAC layer.
| Attribute | Size | Default Value | Description |
|---|---|---|---|
| MAC_PIB_MAX_BE | 8 bits | 8 | Maximum value of back-off exponent. It should always be greater or equal than macMinBE. |
| MAC_PIB_BSN | 8 bits | Random | Beacon frame sequence number |
| MAC_PIB_DSN | 8 bits | Random | Data or command frame sequence number |
| MAC_PIB_MAX_CSMA_BACKOFFS | 8 bits | 50 | Maximum number of back-off attempts |
| MAC_PIB_MIN_BE | 8 bits | 3 | Minimum value of back-off exponent |
| MAC_PIB_MAX_FRAME_RETRIES | 8 bits | 5 | Maximum number of retransmission |
| MAC_PIB_TIMESTAMP_SUPPORTED | 8 bits (bool) | True | MAC frame time stamp support enable (read only) |
| MAC_PIB_SECURITY_ENABLED | 8 bits (bool) | True | Security enabled |
| MAC_PIB_FRAME_COUNTER | 32 bits | 0 | The outgoing frame counter for this device |
| MAC_PIB_DUPLICATE_DETECTION_TTL | 8 bits | 3 | Time a received tuple is retained for duplicate frame detection, in seconds |
| MAC_PIB_HIGH_PRIORITY_WINDOW_SIZE | 8 bits | 7 | The high priority contention window size in number of slots |
| MAC_PIB_TX_DATA_PACKET_COUNT | 32 bits | 0 | Statistic counter of successfully transmitted unicast MSDUs |
| MAC_PIB_RX_DATA_PACKET_COUNT | 32 bits | 0 | Statistic counter of successfully received unicast MSDUs |
| MAC_PIB_TX_CMD_PACKET_COUNT | 32 bits | 0 | Statistic counter of successfully transmitted command packets |
| MAC_PIB_RX_CMD_PACKET_COUNT | 32 bits | 0 | Statistic counter of successfully received command packets |
| MAC_PIB_CSMA_FAIL_COUNT | 32 bits | 0 | Counts the number of times the CSMA backoffs reach macMaxCSMABackoffs |
| MAC_PIB_CSMA_NO_ACK_COUNT | 32 bits | 0 | Counts the number of times an ACK is not received while transmitting a unicast data frame |
| MAC_PIB_RX_DATA_BROADCAST_COUNT | 32 bits | 0 | Statistic counter of successfully received broadcast frames |
| MAC_PIB_TX_DATA_BROADCAST_COUNT | 32 bits | 0 | Statistic counter of the number of broadcast frames sent |
| MAC_PIB_BAD_CRC_COUNT | 32 bits | 0 | Statistic counter of the number of frames received with bad CRC |
| MAC_PIB_NEIGHBOUR_TABLE | 16 Byte entries | Empty | The Neighbour table defined in G3 Spec |
| MAC_PIB_FREQ_NOTCHING | 8 bits (bool) | False | Indicates whether certain frequencies are notched so no signal is injected on them |
| MAC_PIB_CSMA_FAIRNESS_LIMIT | 8 bits | 25 | Channel access fairness limit. Specifies how many failed backoff attempts, back-off exponent is set to minBE |
| MAC_PIB_TMR_TTL | 8 bits | 10 | Maximum time to live for an entry in the neighbour table in minutes |
| MAC_PIB_TONE_MASK | 9 Byte array | All Tones Enabled | Defines the tone mask to use during symbol formation. The value shall be identical for all nodes of a PAN. Inconsistency will cause complete loss of communication. |
| MAC_PIB_BEACON_RANDOMIZATION_WINDOW_LENGTH | 8 bits | 12 | Duration time in seconds for beacon randomization |
| MAC_PIB_A | 8 bits | 8 | This parameter controls the adaptive CW linear decrease |
| MAC_PIB_K | 8 bits | 5 | Rate adaptation factor for channel access fairness limit |
| MAC_PIB_MIN_CW_ATTEMPTS | 8 bits | 255 | Number of consecutive attempts while using minimum CW |
| MAC_PIB_CENELEC_LEGACY_MODE | 8 bits | 1 | This read only attribute indicates the capability of the node. See G3 Spec. |
| MAC_PIB_FCC_LEGACY_MODE | 8 bits | 1 | This read only attribute indicates the capability of the node. See G3 Spec. |
| MAC_PIB_BROADCAST_MAX_CW_ENABLE | 8 bits (bool) | False | If enabled, MAC uses maximum contention window for broadcast frames |
| MAC_PIB_TRANSMIT_ATTEN | 8 bits | 0 | Attenuation of the output level in dB |
| MAC_PIB_POS_TABLE | 5 Byte entries | Empty | The POS table defined in G3 Spec |
| MAC_PIB_POS_RECENT_ENTRIES | 16 bits | 1 | Number of POS table entries having been refreshed recently and which LQI is above adpTrickleLQIThresholdLow |
| MAC_PIB_PLC_DISABLE | 8 bits (bool) | False | Disable PLC PHY Tx and Rx |
| MAC_PIB_PREAMBLE_LENGTH | 8 bits | 8 | Number of P symbols to use in PHY Preamble |
| MAC_PIB_MANUF_DEVICE_TABLE | 6 Byte entries | Empty | The Device table as defined in G3 Spec |
| MAC_PIB_MANUF_NEIGHBOUR_TABLE_ELEMENT | 16 Byte entries | N/A | Provides access to Neighbour table using short address as index |
| MAC_PIB_MANUF_BAND_INFORMATION | 11 Byte struct | Depnds on Band | Maximum number of tones used by the band |
| MAC_PIB_MANUF_COORD_SHORT_ADDRESS | 16 bits | 0x0000 | Short address of the PAN Coordinator |
| MAC_PIB_MANUF_MAX_MAC_PAYLOAD_SIZE | 16 bits | 400 | Maximum payload supported by MAC (read only) |
| MAC_PIB_MANUF_SECURITY_RESET | 8 bits (bool) | N/A | Resets the Device table upon a GMK activation (write only) |
| MAC_PIB_MANUF_FORCED_MOD_SCHEME | 8 bits | 0 | Forces Modulation Scheme in every transmitted frame. 0 - Not forced, 1 - Force Differential, 2 - Force Coherent. |
| MAC_PIB_MANUF_FORCED_MOD_TYPE | 8 bits | 0 | Forces Modulation Type in every transmitted frame. 0 - Not forced, 1 - Force BPSK_ROBO, 2 - Force BPSK, 3 - Force QPSK, 4 - Force 8PSK. |
| MAC_PIB_MANUF_FORCED_TONEMAP | 3 Byte array | All 0's | Forces ToneMap in every transmitted frame. {0} - Not forced, other value will be used as tonemap. |
| MAC_PIB_MANUF_FORCED_MOD_SCHEME_ON_TMRESPONSE | 8 bits | 0 | Forces Modulation Scheme bit in Tone Map Response. 0 - Not forced, 1 - Force Differential, 2 - Force Coherent. |
| MAC_PIB_MANUF_FORCED_MOD_TYPE_ON_TMRESPONSE | 8 bits | 0 | Forces Modulation Type bits in Tone Map Response. 0 - Not forced, 1 - Force BPSK_ROBO, 2 - Force BPSK, 3 - Force QPSK, 4 - Force 8PSK. |
| MAC_PIB_MANUF_FORCED_TONEMAP_ON_TMRESPONSE | 3 Byte array | All 0's | Forces ToneMap field Tone Map Response. {0} - Not forced, other value will be used as tonemap field. |
| MAC_PIB_MANUF_LAST_RX_MOD_SCHEME | 8 bits | N/A | Gets Modulation Scheme of last received frame |
| MAC_PIB_MANUF_LAST_RX_MOD_TYPE | 8 bits | N/A | Gets Modulation Scheme of last received frame |
| MAC_PIB_MANUF_LBP_FRAME_RECEIVED | 8 bits (bool) | 0 | Indicates whether an LBP frame has been received since IB was set to 0 |
| MAC_PIB_MANUF_LNG_FRAME_RECEIVED | 8 bits (bool) | 0 | Indicates whether an LNG frame has been received since IB was set to 0 |
| MAC_PIB_MANUF_BCN_FRAME_RECEIVED | 8 bits (bool) | 0 | Indicates whether an Beacon frame has been received since IB was set to 0 |
| MAC_PIB_MANUF_NEIGHBOUR_TABLE_COUNT | 16 bits | N/A | Gets number of valid elements in the Neighbour Table |
| MAC_PIB_MANUF_RX_OTHER_DESTINATION_COUNT | 32 bits | 0 | Gets number of discarded packets due to Other Destination |
| MAC_PIB_MANUF_RX_INVALID_FRAME_LENGTH_COUNT | 32 bits | 0 | Gets number of discarded packets due to Invalid Frame Length |
| MAC_PIB_MANUF_RX_MAC_REPETITION_COUNT | 32 bits | 0 | Gets number of discarded packets due to MAC Repetition |
| MAC_PIB_MANUF_RX_WRONG_ADDR_MODE_COUNT | 32 bits | 0 | Gets number of discarded packets due to Wrong Addressing mode |
| MAC_PIB_MANUF_RX_UNSUPPORTED_SECURITY_COUNT | 32 bits | 0 | Gets number of discarded packets due to Unsupported Security |
| MAC_PIB_MANUF_RX_WRONG_KEY_ID_COUNT | 32 bits | 0 | Gets number of discarded packets due to Wrong Key Id |
| MAC_PIB_MANUF_RX_INVALID_KEY_COUNT | 32 bits | 0 | Gets number of discarded packets due to Invalid Key |
| MAC_PIB_MANUF_RX_WRONG_FC_COUNT | 32 bits | 0 | Gets number of discarded packets due to Wrong Frame Counter |
| MAC_PIB_MANUF_RX_DECRYPTION_ERROR_COUNT | 32 bits | 0 | Gets number of discarded packets due to Decryption Error |
| MAC_PIB_MANUF_RX_SEGMENT_DECODE_ERROR_COUNT | 32 bits | 0 | Gets number of discarded packets due to Segment Decode Error |
| MAC_PIB_MANUF_ENABLE_MAC_SNIFFER | 8 bits (bool) | False | Enables MAC Sniffer |
| MAC_PIB_MANUF_POS_TABLE_COUNT | 16 bits | N/A | Gets number of valid elements in the POS Table |
| MAC_PIB_MANUF_RETRIES_LEFT_TO_FORCE_ROBO | 8 bits | 0 | Gets or Sets number of retires left before forcing ROBO mode |
| MAC_PIB_MANUF_MAC_INTERNAL_VERSION | 6 Byte struct | Current Version | Gets internal MAC version |
| MAC_PIB_MANUF_MAC_RT_INTERNAL_VERSION | 6 Byte struct | Current Version | Gets internal MAC RT version |
| MAC_PIB_MANUF_RESET_MAC_STATS | 8 bits (bool) | 0 | Resets MAC statistics |
| MAC_PIB_MANUF_MAC_RT_SLEEP_MODE | 8 bits (bool) | 0 | Enable/Disable Sleep mode |
| MAC_PIB_MANUF_MAC_RT_DEBUG_SET | 7 bytes | All 0's | Configures Debug mode to read memory from PLC device |
| MAC_PIB_MANUF_MAC_RT_DEBUG_READ | 144 bytes | All 0's | Read memory from PLC device. Address configured through MAC_WRP_PIB_MANUF_DEBUG_SET |
| MAC_PIB_MANUF_POS_TABLE_ELEMENT | 5 Byte entries | N/A | Provides access to POS table using short address as index |
| MAC_PIB_MANUF_TRICKLE_MIN_LQI | 8 bits | 80 | Minimum LQI to consider a neighbour for Trickle |
| MAC_PIB_MANUF_NEIGHBOUR_LQI | 8 bits | N/A | LQI for a given neighbour, which short address will be indicated as index |
| MAC_PIB_MANUF_BEST_LQI | 8 bits | N/A | Best LQI found in neighbour table |
| MAC_PIB_MANUF_PLC_IFACE_AVAILABLE | 8 bits (bool) | N/A | PLC Interface availability |
| MAC_PIB_MANUF_LAST_FRAME_DURATION_PLC | 16 bits | N/A | Last PLC frame duration in ms |
| MAC_PIB_MANUF_RESET_TMR_TTL | 8 bits | N/A | Resets TMR TTL for the Short Address contained in Index |
| MAC_PIB_MANUF_PHY_PARAM | Variable | N/A | Gets or sets a parameter in Phy layer. Index will be used to contain PHY parameter ID. See MAC_WRP_PHY_PARAM. |
Remarks
None.