1.3.4.1.4 MAC_PLC_Status Function
C
SYS_STATUS MAC_PLC_Status
(
void
);
Summary
The MAC_PLC_Status primitive retrieves the Status of PLC MAC.
Description
This primitive is intended to be called before using PLC MAC layer to ensure it is ready to be used.
Precondition
MAC_PLC_Init must have been called before calling this function.
Parameters
None.
Returns
Status of PLC MAC layer as a SYS_STATUS code.
Example
SYS_STATUS status;
status = MAC_PLC_Status();
if (status == SYS_STATUS_READY)
{
// MAC is ready to be used
}
Remarks
None.