1.3.5.1.21 MAC_RF_RLQ_IE Struct

C

typedef struct
{
    MAC_RF_HEADER_IE headerIE;
    uint8_t reverseLqi;
} MAC_RF_RLQ_IE;

Summary

Defines the fields of the MAC Reverse Link Quality Information Element.

Description

This structure contains the fields of a MAC Reverse Link Quality Information Element, as defined in the G3-PLC standard.

Field description:

  • headerIE: The Information Element Header
  • reverseLqi: Quality of received frames from the destination of the packet containing this IE, as seen by the transmitter of the packet containing this IE

Remarks

None.