4.11 Controlling Debug Log Levels for the WILCS02 Driver
The WILCS02 driver inherits the debug logs levels from Linux. To
manage these debug levels, the user can follow any of the following procedures:
- Changing the system debug level
- Using
debugfsto control specific debug regions
Changing the System Debug Level
- The user can change the debug level by executing the following
command”
#echo "7" > /proc/sys/kernel/printkNote: Where,“7”is the highest desired log level. - The following command sets the debug
level:
# dmesg -n 7 - To change the default log level while building the kernel, the user can
modify the following line in
kernel_src/include/linux/printk.h.#define CONSOLE_LOGLEVEL_DEFAULT 7
Using debugfs to Control Debug Regions
The WILCS02 driver also uses
debugfs
to allow the user to control which code regions have enabled or disabled logs. The
following are the steps to manage debug regions.- The user must mount the
debugfsusing the following command:# mount -t debugfs nodev /sys/kernel/debug - Echo a number that represents a bit field of the regions to enable logs
from. The bit field is defined as
follows:
BIT 0: GENERIC BIT 1: HOSTAPD BIT 2: HOSTINF BIT 3: CORECONFIG BIT 4: CFG80211 BIT 5: INT BIT 6: TX BIT 7: RX BIT 8: TCP BIT 9: INIT BIT 10: PWRDEV