4.3 Working with SDIO Interface
The device tree configuration for SDIO bus is enabled by default. The kernel installs the
WILCS02 SDIO driver when it detects the SD board. The
following log is displayed upon successful driver
installation:
mmc0: new high speed SDIO card at address 0001
wilc_sdio mmc0:0001:1: SDIO single driver speed: 50000000
wilc_sdio mmc0:0001:1: chipid 00000053
loading firmware mchp/wilcs02_wifi_firmware.bin
Downloading Firmware ...
The best firmware already installed on WILCS02
Download Succeeded
wilc_sdio mmc0:0001:1: Driver Initializing successIf the kernel does not automatically install the driver, the user can manually install
the WILCS02 SDIO driver using the following
command:
modprobe wilc-sdio
After executing the command, the driver initialization log must appear (see SDIO Card
Detection and Driver Initialization Log). Verify the driver installation by
listing the loaded modules with the
lsmod
command:# lsmod Module Size Used by cfg80211 307200 0 atmel_usba_udc 20480 0
To manually load the WILCS02 SDIO driver, use the following
command:
# modprobe wilc-sdio wilc_sdio mmc0:0001:1: SDIO single driver speed: 50000000 wilc_sdio mmc0:0001:1: chipid 00000053 loading firmware mchp/wilcs02_wifi_firmware.bin Downloading Firmware ... The best firmware already installed on WILCS02 Download Succeeded wilc_sdio mmc0:0001:1: Driver Initializing success
Note:
- Ensure that the device tree configuration for the SDIO bus is enabled in the system.
- The log messages provide critical information about the driver installation process and can help in troubleshooting any issues.