4.6 Modifying Configuration Files

To use the Wi-Fi® module, the user must load a set of default configuration files on the pre-built image. The user can also modify these files as per the requirement described in the following sections.