2.7 Run PROGRAM Action
(Ask a Question)After generating the bitstream, the PolarFire device must be programmed. To program the PolarFire device, perform the following steps:
- Ensure that the following Jumper
Settings are set on the board, which will be used as the Root Port device.
Table 2-2. Jumper Settings Jumper Description Default J18, J19, J20, J21, and J22 Short pin 2 and 3 for programming the PolarFire® FPGA through FTDI Closed J28 Short pins 1 and 2 for programming through the on-board FlashPro5 Open J4 Short pins 1 and 2 for manual power switching using SW3 Closed J12 Short pins 3 and 4 for 2.5V Closed - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- On the Libero in the Design Flow tab, double click Run PROGRAM Action.
When the device is programmed successfully, a green tick mark appears as shown Figure 2-1. The device is successfully programmed, see Setting Up the Demo.