2 Libero Design Flow
(Ask a Question)This section describes the Libero design flow for running this demo.
Important:
- To initialize the TCM in
PolarFire using the system controller, change the local parameter,
l_cfg_hard_tcm0_en, to 1’b1 in the
miv_rv32_opsrv_cfg_pkg.vfile prior to synthesis. See the 2.7 TCM section in the MIV_RV32 v3.0 Handbook from the Libero SoC Catalog. - To run the Libero design using TCL script, see Appendix 2: Running the TCL Script.
The following figure shows these options in the Design Flow tab.