9 Revision History

RevisionDateDescription
B05/2023The following is the list of changes in revision B of the document:
A07/2022The following is the list of changes in revision A of the document:
  • The document was migrated to the Microchip template.
  • The document number was updated to DS00004623 from 50200799.
  • Updated the document for Libero® SoC v2022.1
5.0—Added Appendix 2: Running the TCL Script.
4.0—

The following is a summary of the changes made in this revision.

  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
3.0—

The following is a summary of changes made in this revision.

  • Updated the document for Libero SoC v12.1.
  • The design uses a new IP PF_IOD_CDR_CCC. For more information, see PF_IOD_CDR_CCC_C0.
2.0—

The following is a summary of changes made in this revision.

1.0—This is the first publication of the document.