2.9.4.1 USB_DEVICE_PRINTER_EventHandlerSet Function
C
USB_DEVICE_PRINTER_RESULT USB_DEVICE_PRINTER_EventHandlerSet(
USB_DEVICE_PRINTER_INDEX instanceIndex,
USB_DEVICE_PRINTER_EVENT_HANDLER eventHandler,
uintptr_t context
);
Summary
This function registers a event handler for the specified PRINTER function driver instance. This function should be called by the client when it receives a SET CONFIGURATION event from the device layer. A event handler must be registered for function driver to respond to function driver specific commands. If the event handler is not registered, the device layer will stall function driver specific commands and the USB device may not function.
Precondition
This function should be called when the function driver has been initialized as a result of a set configuration.
Parameters
| Parameters | Description |
| instanceIndex | Instance of the PRINTER Function Driver. |
| eventHandler | A pointer to event handler function. |
| context | Application specific context that is returned in the event handler. |
Returns
USB_DEVICE_PRINTER_RESULT_OK - The operation was successful
USB_DEVICE_PRINTER_RESULT_ERROR_INSTANCE_INVALID - The specified instance does not exist
USB_DEVICE_PRINTER_RESULT_ERROR_PARAMETER_INVALID - The eventHandler parameter is NULL
Example
// This code snippet shows an example registering an event handler. Here
// the application specifies the context parameter as a pointer to an
// application object (appObject) that should be associated with this
// instance of the PRINTER function driver.
// Application states
typedef enum
{
//Application's state machine's initial state.
APP_STATE_INIT=0,
APP_STATE_SERVICE_TASKS,
APP_STATE_WAIT_FOR_CONFIGURATION,
} APP_STATES;
USB_DEVICE_HANDLE usbDeviceHandle;
APP_STATES appState;
USB_DEVICE_PRINTER_RESULT result;
USB_DEVICE_PRINTER_EVENT_RESPONSE APP_USBDevicePrinterEventHandler
(
USB_DEVICE_PRINTER_INDEX instanceIndex ,
USB_DEVICE_PRINTER_EVENT event ,
void* pData,
uintptr_t context
)
{
// Event Handling comes here
switch(event)
{
case USB_DEVICE_PRINTER_EVENT_READ_COMPLETE:
// This means that the host has sent some data to the device
break;
case USB_DEVICE_PRINTER_EVENT_WRITE_COMPLETE:
// This means that the host has received some data from device
break;
default:
break;
}
return USB_DEVICE_PRINTER_EVENT_RESPONSE_NONE;
}
// This is the application device layer event handler function.
USB_DEVICE_EVENT_RESPONSE APP_USBDeviceEventHandler
(
USB_DEVICE_EVENT event,
void * pData,
uintptr_t context
)
{
USB_SETUP_PACKET * setupPacket;
switch(event)
{
case USB_DEVICE_EVENT_POWER_DETECTED:
// This event in generated when VBUS is detected. Attach the device
USB_DEVICE_Attach(usbDeviceHandle);
break;
case USB_DEVICE_EVENT_POWER_REMOVED:
// This event is generated when VBUS is removed. Detach the device
USB_DEVICE_Detach (usbDeviceHandle);
break;
case USB_DEVICE_EVENT_CONFIGURED:
// This event indicates that Host has set Configuration in the Device.
// Register PRINTER Function driver Event Handler.
USB_DEVICE_PRINTER_EventHandlerSet(USB_DEVICE_PRINTER_INDEX_0, APP_USBDevicePRINTEREventHandler, (uintptr_t)0);
break;
case USB_DEVICE_EVENT_CONTROL_TRANSFER_SETUP_REQUEST:
// This event indicates a Control transfer setup stage has been completed.
setupPacket = (USB_SETUP_PACKET *)pData;
// Parse the setup packet and respond with a USB_DEVICE_ControlSend(),
// USB_DEVICE_ControlReceive or USB_DEVICE_ControlStatus().
break;
case USB_DEVICE_EVENT_CONTROL_TRANSFER_DATA_SENT:
// This event indicates that a Control transfer Data has been sent to Host.
break;
case USB_DEVICE_EVENT_CONTROL_TRANSFER_DATA_RECEIVED:
// This event indicates that a Control transfer Data has been received from Host.
break;
case USB_DEVICE_EVENT_CONTROL_TRANSFER_ABORTED:
// This event indicates a control transfer was aborted.
break;
case USB_DEVICE_EVENT_SUSPENDED:
break;
case USB_DEVICE_EVENT_RESUMED:
break;
case USB_DEVICE_EVENT_ERROR:
break;
case USB_DEVICE_EVENT_RESET:
break;
case USB_DEVICE_EVENT_SOF:
// This event indicates an SOF is detected on the bus. The USB_DEVICE_SOF_EVENT_ENABLE
// macro should be defined to get this event.
break;
default:
break;
}
}
void APP_Tasks ( void )
{
// Check the application's current state.
switch ( appState )
{
// Application's initial state.
case APP_STATE_INIT:
// Open the device layer
usbDeviceHandle = USB_DEVICE_Open( USB_DEVICE_INDEX_0,
DRV_IO_INTENT_READWRITE );
if(usbDeviceHandle != USB_DEVICE_HANDLE_INVALID)
{
// Register a callback with device layer to get event notification
USB_DEVICE_EventHandlerSet(usbDeviceHandle,
APP_USBDeviceEventHandler, 0);
appState = APP_STATE_WAIT_FOR_CONFIGURATION;
}
else
{
// The Device Layer is not ready to be opened. We should try
// gain later.
}
break;
case APP_STATE_SERVICE_TASKS:
break;
// The default state should never be executed.
default:
break;
}
}
Remarks
None.