7 PMBus Commands
| No. | Name | Adr. | No. | Name | Adr. | No. | Name | Adr. | ||
|---|---|---|---|---|---|---|---|---|---|---|
| 1 | OPERATION | 0x01 | 18 | VOUT_OV_FAULT_RESPONSE | 0x41 | 35 | STATUS_BYTE | 0x78 | ||
| 2 | ON_OFF_CONFIG | 0x02 | 19 | VOUT_OV_WARN_LIMIT | 0x42 | 36 | STATUS_WORD | 0x79 | ||
| 3 | CLEAR_FAULTS | 0x03 | 20 | VOUT_UV_WARN_LIMIT | 0x43 | 37 | STATUS_VOUT | 0x7A | ||
| 4 | WRITE_PROTECT | 0x10 | 21 | VOUT_UV_FAULT_LIMIT | 0x44 | 38 | STATUS_IOUT | 0x7B | ||
| 5 | STORE_USER_ALL | 0x15 | 22 | VOUT_UV_FAULT_RESPONSE | 0x45 | 39 | STATUS_INPUT | 0x7C | ||
| 6 | RESTORE_USER_ALL | 0x16 | 23 | IOUT_OC_FAULT_LIMIT | 0x46 | 40 | STATUS_TEMPERATURE | 0x7D | ||
| 7 | CAPABILITY | 0x19 | 24 | IOUT_OC_FAULT_RESPONSE | 0x47 | 41 | STATUS_CML | 0x7E | ||
| 8 | SMBALERT_MASK | 0x1B | 25 | VIN_OV_FAULT_LIMIT | 0x55 | 42 | READ_VIN | 0x88 | ||
| 9 | VOUT_MODE | 0x20 | 26 | VIN_OV_FAULT_RESPONSE | 0x56 | 43 | READ_VOUT | 0x8B | ||
| 10 | VOUT_COMMAND | 0x21 | 27 | VIN_UV_WARN_LIMIT | 0x58 | 44 | READ_TEMPERATURE | 0x8D | ||
| 11 | VOUT_MAX | 0x24 | 28 | POWER_GOOD_ON | 0x5E | 45 | PMBUS_REVISION | 0x98 | ||
| 12 | VOUT_MARGIN_HIGH | 0x25 | 29 | TON_DELAY | 0x60 | 46 | MFR_ID | 0x99 | ||
| 13 | VOUT_MARGIN_LOW | 0x26 | 30 | TON_RISE | 0x61 | 47 | MFR_MODEL | 0x9A | ||
| 14 | VOUT_TRANSITION_RATE | 0x27 | 31 | TON_MAX_FAULT_LIMIT | 0x62 | 48 | MFR_REVISION | 0x9B | ||
| 15 | VIN_ON | 0x35 | 32 | TON_MAX_FAULT_RESPONSE | 0x63 | 49 | IC_DEVICE_ID | 0xAD | ||
| 16 | VIN_OFF | 0x36 | 33 | TOFF_DELAY | 0x64 | 50 | IC_DEVICE_REV | 0xAE | ||
| 17 | VOUT_OV_FAULT_LIMIT | 0x40 | 34 | TOFF_FALL | 0x65 | |||||
OPERATION (0x01)
The OPERATION command is used to turn the device output ON or OFF. It is also used to set the output voltage to the upper or lower MARGIN voltages.
| COMMAND | OPERATION | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: Controls if PMBus device output is ON or OFF
- 0 : Output is OFF
- 1 : Output is ON
Bit [6]: Controls the power down behavior
- 0 : Output is turned OFF immediately
- 1 : The device is powered down following the values set in the TOFF_DELAY and TOFF_FALL commands
Bit [5:4]: Voltage command source
- 00 : The nominal output voltage is set by the PMBus VOUT_COMMAND data
- 01 : The nominal output voltage is set by the PMBus VOUT_MARGIN_LOW data
- 10 : The nominal output voltage is set by the PMBus VOUT_MARGIN_HIGH data
- 11 : AVS Bus (AVS Bus not supported)
Bit [3:2]: Margin fault response
- 00 : Invalid
- 01 : The faults caused by VOUT_MARGIN_HIGH or VOUT_MARGIN_LOW are ignored
- 10 : The faults caused by VOUT_MARGIN_HIGH or VOUT_MARGIN_LOW are acted upon
- 11 : Invalid
Bit [1]: Transition control (AVS Bus not implemented)
Bit [0]: Reserved
ON_OFF_CONFIG (0x02)
| COMMAND | ON_OFF_CONFIG | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 1 |
Bit [7:5]: Reserved
Bit [4]: Sets the default to either operate when power is present or for the ON/OFF to be controlled by serial bus commands
- 0 : Device powers up when the power is present
- 1 : Device does not power up until commanded by the OPERATION command
Bit [3]: Controls how the unit responds to commands received via the serial bus
- 0 : Device ignores the ON/OFF portion of the OPERATION command from serial bus
- 1 : Device requires the ON/OFF portion of the OPERATION command
Bit [2]: Controls how the unit responds to the EN pin
- 0 : Unit ignores the EN pin (ON/OFF controlled only the OPERATION command)
- 1 : Unit requires the EN pin to be asserted to start the unit
Bit [1]: Polarity of the EN pin
- 0 : Active low
- 1 : Active high
Bit [0]: EN pin action
- 0 : Use the programmed turn OFF delay and fall time
- 1 : Turn OFF the output and stop transferring energy to the output as fast as possible
CLEAR_FAULTS (0x03)
The CLEAR_FAULTS command is used to clear any fault bits that have been set. This command clears all bits in all status registers simultaneously. At the same time, the device releases its SMBALERT signal output if the device is asserting the SMBALERT signal. The CLEAR_FAULTS command does not cause a unit that has latched off for a fault condition to restart. If the fault is still present when the bit is cleared, the fault bit is immediately reset and the host notified by the usual means.
WRITE_PROTECT (0x10)
| COMMAND | WRITE_PROTECT | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: Control writing to the PMBus device for protection against accidental changes
- 0 : Enable all writes as permitted in bit 5 or bit 6
- 1 : Disable all writes except the WRITE_PROTECT command (bit 5 and bit 6 must be 0)
Bit [6]: Control writing to the PMBus device for protection against accidental changes
- 0 : Enable all writes as permitted in bit 5 or bit 7
- 1 : Disable all writes except for the WRITE_PROTECT, and OPERATION commands (bit 5 and bit 7 must be 0)
Bit [5]: Control writing to the PMBus device for protection against accidental changes
- 0 : Enable all writes as permitted in bit 6 or bit 7
- 1 : Disable all writes except the WRITE_PROTECT, OPERATION, ON_OFF_CONFIG, and VOUT_COMMAND. (bit 6 and bit 7 must be 0)
Bit [4:0]: Reserved
STORE_USER_ALL (0x15)
The STORE_USER_ALL command stores all of the current storable register settings in the EEPROM memory as the new defaults on power up. It is permissible to use this command while the device is switching. To use this command:
- Set all settings to the desired power up configuration.
- Pull EN low to disable switching.
- Apply 7.5 ± 0.25V to the VIN pin
- Execute the command.
- Execute a RESTORE_USRE_ALL command..
- Compare the settings in the part values with the expected settings. If they differ, repeat this procedure. If the settings differ a second time, discard the part.
RESTORE_USER_ALL (0x16)
The RESTORE_USER_ALL command restores all of the storable register settings from EEPROM memory to those registers which are unprotected. This command should not be used while the part is converting power.
CAPABILITY (0x19)
| COMMAND | CAPABILITY | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 0 |
Bit [7]: Packet Error Checking
- 0 : Packet Error Checking not supported
Bit [6:5]: Maximum Bus Speed
- 01 : Maximum supported bus speed is 400 kHz
Bit [4]: SMBALERT#
- 1 : Enable the SMBus Alert Response protocol
Bit [3]: Numeric Format
- 0 : Numeric data is in LINEAR11, ULINEAR16, SLINEAR16
Bit [2]: AVSBus Support
- 0 : AVSBus not supported
Bit [1:0]: Reserved
SMBALERT_MASK (0x1B)
The SMBALERT_MASK command may be used to prevent a warning or fault condition from asserting the SMBALERT# signal. The bits in the mask byte align with the bits in the corresponding status register. For example if the STATUS_TEMPERATURE command code were sent with the mask byte 01000000b, then an Overtemperature Warning condition would be blocked from asserting SMBALERT#. This command cannot be used with STATUS_BYTE or STATUS_WORD. Since these commands are the logical or of underlying status registers, use the underlying status commands as the status command code sent to set a mask value. The access mode is a write word transaction for the write and a block write block read transaction for reading. Refer to the SMBus specification for details on this transaction.
VOUT_MODE (0x20)
The data byte for the VOUT_MODE command is one byte that consists of bit [7:5] as Mode and bit[4:0] as Exponent Parameter. The three-bit Mode sets whether the device uses the ULINEAR16, Half-precision IEEE 754 floating point, VID or DIRECT modes for output voltage related commands. The five-bit Parameter provides more information about the selected mode.
| COMMAND | VOUT_MODE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 1 | 0 | 0 | 1 | 1 | 0 | 0 | 0 |
Bit [7]: Data type
- 1 : Device supports relative mode
Bit [6:5]: Data type
- 00 : Five bit two’s complement exponent for the mantissa delivered as the data bytes for an output voltage related command
Bit [4:0]: Exponent parameter
VOUT_COMMAND (0x21)
The VOUT_COMMAND command sets the output voltage in volts
| COMMAND | VOUT_COMMAND | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 1 | 0 | 1 | 0 |
Bit [15:0]: Two linear16 data bytes
Note that this part does not use VOUT_SCALE_LOOP. The value provided via the VOUT_COMMAND command is the voltage that the part will regulate the FB pin to. Any voltage divider used on that pin will need to be accounted for by the user when using VOUT_COMMAND.
VOUT_MAX (0x24)
The VOUT_MAX command sets the maximum output voltage. The purpose is to protect the devices on the output rail supplied by this device from a higher than acceptable output voltage
| COMMAND | VOUT_MAX | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [15:0]: Two linear 16 data bytes
VOUT_MARGIN_HIGH (0x25)
This VOUT_MARGIN_HIGH command loads the unit with the voltage to which the output is to be changed when the OPERATION command is set to “Margin High.”
| COMMAND | VOUT_MARGIN_HIGH | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 1 |
Bit [15:0]: Two linear 16 data bytes
VOUT_MARGIN_LOW (0x26)
This VOUT_MARGIN_LOW command loads the unit with the voltage to which the output is to be changed when the OPERATION command is set to “Margin Low.”
| COMMAND | VOUT_MARGIN_LOW | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0 | 0 | 1 | 1 | 0 |
Bit [15:0]: Two linear 16 data bytes
VOUT_TRANSITION_RATE (0x27)
VOUT_TRANSITION_RATE command sets the rate in mV/μs at which the output should change voltage.
| COMMAND | VIN_ON | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
Bits [15:11]: A 5 bit, two’s complement exponent for the calculation, fixed at -2
Bits [10:0]: An 11 bit, two’s complement mantissa for the calculation
Valid range: 0 to 31.75 V/ms
VIN_ON (0x35)
The VIN_ON command sets the value of the input voltage, in Volts, at which the unit should start power conversion.
| COMMAND | VIN_ON | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 |
Bits [15:11]: A 5 bit, two’s complement exponent, fixed at -1.
Bits [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0V to 15.5V
VIN_OFF (0x36)
The VIN_OFF command sets the value of the input voltage, in Volts, at which the unit, once operation has started, should stop power conversion.
| COMMAND | VIN_OFF | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 |
Bits [15:11]: A 5 bit, two’s complement exponent, fixed at -1
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0V to 15.5V
VOUT_OV_FAULT_LIMIT (0x40)
The VOUT_OV_FAULT_LIMIT command sets the value of the output voltage measured at the sense or output pins that causes an output overvoltage fault.
| COMMAND | VOUT_OV_FAULT_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 relative format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 |
Bit [15:0]: A 16 bit, two’s complement integer
VOUT_OV_FAULT_RESPONSE (0x41)
The VOUT_OV_FAULT_RESPONSE command instructs the device on what action to take in response to an output overvoltage fault
| COMMAND | VOUT_OV_FAULT_RESPONSE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Valid values:
0x00: Continue without interruption
0x80: Shuts down and does not attempt to restart
0xC0: Shuts down and attempts to restart when the fault condition is no longer present
VOUT_OV_WARN_LIMIT (0x42)
The VOUT_OV_WARN_LIMIT command sets the value of the output voltage at the sense or output pins that causes an output voltage high warning. This value is typically less than the output overvoltage threshold.
| COMMAND | VOUT_OV_WARN_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 relative format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | 1 | 1 | 0 |
Bit [15:0]: A 16 bit, two’s complement integer
VOUT_UV_WARN_LIMIT (0x43)
The VOUT_UV_WARN_LIMIT command sets the value of the output voltage at the sense or output pins that causes an output voltage low warning. This value is typically greater than the output undervoltage fault threshold.
| COMMAND | VOUT_UV_WARN_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 relative format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 1 | 1 | 0 | 0 | 1 |
Bit [15:0]: A 16 bit, two’s complement integer
VOUT_UV_FAULT_LIMIT (0x44)
The VOUT_UV_FAULT_LIMIT command sets the value of the output voltage at the sense or output pins that causes an output undervoltage fault. This fault is masked until the unit reaches the programmed output voltage. This fault is also masked when the unit is disabled.
| COMMAND | VOUT_UV_FAULT_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 relative format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 | 0 | 0 |
Bit [15:0]: A 16 bit, two’s complement integer
VOUT_UV_FAULT_RESPONSE (0x45)
The VOUT_UV_FAULT_RESPONSE command instructs the device on what action to take in response to an output undervoltage fault
| COMMAND | VOUT_UV_FAULT_RESPONSE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Valid values:
0x00: Continue without interruption
0x80: Shuts down and does not attempt to restart
IOUT_OC_FAULT_LIMIT (0x46)
The IOUT_OC_FAULT_LIMIT command sets the value of the output current, in Amperes, that causes the overcurrent detector to indicate an overcurrent fault condition
| COMMAND | IOUT_OC_FAULT_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 |
Bits [15:11]: A 5 bit, two’s complement exponent, fixed at -1
Bits [10:0]: An 11 bit, two’s complement mantissa
Valid range: 4.5 to 20 A
IOUT_OC_FAULT_RESPONSE (0x47)
The IOUT_OC_FAULT_RESPONSE command instructs the device on what action to take in response to an output overcurrent fault.
| COMMAND | IOUT_OC_FAULT_RESPONSE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 |
Valid values:
0xC0: Shuts down and does not attempt to restart
0xF8: Shuts down and attempts to restart continuously
VIN_OV_FAULT_LIMIT (0x55)
The VIN_OV_FAULT_LIMIT command sets the value of the input voltage that causes an Input Overvoltage Fault.
| COMMAND | VIN_OV_FAULT_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at 0.
Bit [10:0]: An 11 bit, two’s complement mantissa
Maximum value: 18V
VIN_OV_FAULT_RESPONSE (0x56)
The VIN_OV_FAULT_RESPONSE command instructs the device on what action to take in response to an Input Overvoltage Fault.
| COMMAND | VIN_OV_FAULT_RESPONSE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Valid values:
0x00: Continue without interruption
0x80: Shuts down and does not attempt to restart
VIN_UV_WARN_LIMIT (0x58)
The VIN_UV_WARN_LIMIT command sets the value of the input voltage that causes an input voltage low warning. This value is typically greater than the Input Undervoltage Fault threshold, VIN_UV_FAULT_LIMIT
| COMMAND | VIN_UV_WARN_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -1
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0V to 15.5V
POWER_GOOD_ON (0x5E)
The POWER_GOOD_ON command sets the output voltage at which an optional POWER_GOOD signal should be asserted, indicating that the output voltage is valid. Note that depending on the choice of the device manufacturer that a device may drive a POWER_GOOD signal high or low to indicate that the signal is asserted.
| COMMAND | POWER_GOOD_ON | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 16 relative format | |||||||||||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0 | 0 | 1 | 1 | 0 |
Bit [15:0]: Two linear16 data bytes
TON_DELAY (0x60)
The TON_DELAY command sets the time, in milliseconds, from when a start condition is received until the output voltage starts to rise.
| COMMAND | TON_DELAY | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -1
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0 to 127.5ms
TON_RISE (0x61)
The TON_RISE command sets the time, in milliseconds, from when the output starts to rise until the voltage has entered the regulation band. A value of 0 milliseconds instructs the unit to bring its output voltage to the programmed regulation value as quickly as possible.
| COMMAND | TON_RISE | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -2
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0 to 127.75ms
TON_MAX_FAULT_LIMIT (0x62)
The TON_MAX_FAULT_LIMIT command sets an upper limit, in milliseconds, on how long the unit can attempt to power up the output without reaching the output undervoltage fault limit. A value of 0 milliseconds means that there is no limit and that the unit can attempt to bring up the output voltage indefinitely.
| COMMAND | TON_MAX_FAULT_LIMIT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -2
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0 to 127.75ms
TON_MAX_FAULT_RESPONSE (0x63)
The TON_MAX_FAULT_RESPONSE command instructs the device on what action to take in response to a TON_MAX fault.
| COMMAND | TON_MAX_FAULT_RESPONSE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Valid values:
0x00: Continue without interruption
0x80: Shuts down and does not attempt to restart
TOFF_DELAY (0x64)
The TOFF_DELAY command sets the time, in milliseconds, from when a stop condition is received (as programmed by the ON_OFF_CONFIG command) until the unit stops transferring energy to the output.
| COMMAND | TOFF_DELAY | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -1
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0 to 127.5ms
TOFF_FALL (0x65)
The TOFF_FALL command sets the time, in milliseconds, from the end of the turn-OFF delay time until the voltage is commanded to zero. A value of 0 milliseconds means that the device should ramp the output voltage down as fast as it can.
| COMMAND | TOFF_FALL | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R/W, Linear 11 format | |||||||||||||||
| Default # | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 |
Bit [15:11]: A 5 bit, two’s complement exponent, fixed at -2
Bit [10:0]: An 11 bit, two’s complement mantissa
Valid range: 0 to 127.75ms
STATUS_BYTE (0x78)
The STATUS_BYTE command returns one byte of information with a summary of the most critical faults.
| COMMAND | STATUS_BYTE (LOW BYTE of STATUS_WORD) | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: A fault was declared because the device was busy and unable to respond
Bit [6]: This bit is asserted if the unit is not providing power to the output, regardless of the reason, including simply not being enabled
Bit [5]: An output overvoltage fault has occurred
Bit [4]: An output overcurrent fault has occurred
Bit [3]: An input undervoltage fault has occurred
Bit [2]: A temperature fault or warning has occurred
Bit [1]: A communications, memory or logic fault has occurred
Bit [0]: A fault or warning not listed in bits [7:1] has occurred
STATUS_WORD (0x79)
The STATUS_WORD command returns two bytes of information with a summary of the unit’s fault condition. Based on the information in these bytes, the host can get more information by reading the appropriate status registers. The low byte of the STATUS_WORD is the same register as the STATUS_BYTE command.
| COMMAND | STATUS_WORD (HIGH BYTE of STATUS_WORD) | |||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: An output voltage fault or warning has occurred
Bit [6]: An output current fault or warning has occurred.
Bit [5]: An input voltage fault or warning has occurred
Bit [4]: A manufacturer specific fault or warning has occurred
Bit [3]: The POWER_GOOD signal, if present, is negated
Bit [2]: A fan or airflow fault or warning has occurred (not used)
Bit [1]: A bit in STATUS_OTHER is set
Bit [0]: A fault type not given in bits [15:1] of the STATUS_WORD has been detected
STATUS_VOUT (0x7A)
The STATUS_VOUT command returns one byte of information relating to the status of the converter's output voltage related faults
| COMMAND | STATUS_VOUT | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: OUT_OV_FAULT
Bit [6]: VOUT_OV_WARNING
Bit [5]: VOUT_UV_WARNING
Bit [4]: VOUT_UV_FAULT
Bit [3]: VOUT_MAX_MIN Warning
Bit [2]: TON_MAX_FAULT
Bit [1]: TOFF_MAX_WARNING
Bit [0]: VOUT Tracking Error (not used)
STATUS_IOUT (0x7B)
The STATUS_IOUT command returns one byte of information relating to the status of the converter’s output current related faults.
| COMMAND | STATUS_IOUT | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: OUT_OC_FAULT
Bit [6]: IOUT_OC_LV_FAULT
Bit [5]: IOUT_OC_WARNING
Bit [4]: IOUT_UC_FAULT (not used)
Bit [3]: Current Share Fault (not used)
Bit [2]: In Power Limiting Mode (not used)
Bit [1]: POUT_OP_FAULT (not used)
Bit [0]: POUT_OP_WARNING (not used)
STATUS_INPUT (0x7C)
The STATUS_INPUT command returns one byte of information relating to the status of the input-related faults of the converter.
| COMMAND | STATUS_INPUT | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: VIN_OV_FAULT
Bit [6]: VIN_OV_WARNING
Bit [5]: VIN_UV_WARNING
Bit [4]: VIN_UV_FAULT
Bit [3]: Unit OFF For Insufficient Input Voltage
Bit [2]: IIN_OC_FAULT (not used)
Bit [1]: IIN_OC_WARNING (not used)
Bit [0]: PIN_OP_WARNING (not used)
STATUS_TEMPERATURE (0x7D)
The STATUS_TEMPERATURE command returns one byte of information relating to the status of the external temperature related faults.
| COMMAND | STATUS_TEMPERATURE | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: OT_FAULT
Bit [6]: OT_WARNING
Bit [5]: UT_WARNING (not used)
Bit [4]: UT_FAULT (not used)
Bit [3:0]: Reserved
STATUS_CML (0x7E)
The STATUS_CML command returns one byte of information relating to the status of the communication-related faults of the converter.
| COMMAND | STATUS_CML | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit [7]: Invalid or unsupported command received
Bit [6]: Invalid or unsupported data received
Bit [5]: Packet error check failed (not used)
Bit [4]: Memory fault detected
Bit [3]: Processor fault detected
Bit [2]: Reserved
Bit [1]: A communication fault other than the ones listed in this table has occurred
Bit [0]: Other memory or logic fault has occurred
READ_VIN (0x88)
The READ_VIN command returns two bytes of data in the linear data format that represent the input voltage of the converter.
| COMMAND | READ_VIN | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R, Linear 11 format | |||||||||||||||
Bits [15:11]: A two’s complement exponent, -4
Bits [10:0]: An 11 bit two’s complement mantissa
READ_VOUT (0x8B)
The READ_VOUT command returns two bytes of data in the linear data format that represent the output voltage of the converter.
| COMMAND | READ_VOUT | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R, Linear 16 format | |||||||||||||||
Bits [15:0]: A two’s complement mantissa for use with the exponent from VOUT_MODE, -8
READ_TEMPERATURE (0x8D)
The READ_TEMPERATURE command returns the external temperature in degrees Celsius.
| COMMAND | READ_TEMPERATURE | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R, Linear 11 format | |||||||||||||||
Bits [15:11]: A two’s complement exponent, 0
Bits [10:0]: An 11 bit two’s complement mantissa
PMBUS_REVISION (0x98)
PMBUS_REVISION command stores or reads the revision of the PMBus to which the device is compliant.
| COMMAND | PMBUS_REVISION | |||||||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | R | |||||||
| Default # | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 |
Bit [7:4]: Indicate the revision of PMBus specification Part I to which the device is compliant
Bit [3:0]: Indicate the revision of PMBus specification Part II to which the device is compliant
MFR_ID (0x99)
The MFR_ID command is used to either set or read the manufacturer’s ID (name, abbreviation or symbol that identifies the unit’s manufacturer). The actual data for this command is 3 bytes. The high order byte here is the byte count in the SMBus block read and block write transactions.
| COMMAND | MFR_ID | |||||||||||||||
| Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| Access | Block R/W, 4 bytes | |||||||||||||||
| Default # | ||||||||||||||||
| COMMAND | MFR_ID, 4 bytes | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | Block R/W | |||||||||||||||
| Default # | ||||||||||||||||
MFR_MODEL (0x9A)
The MFR_MODEL command is used to either set or read the manufacturer’s model number. The actual data for this command is 1 byte. The high order byte here is the byte count in the SMBus block read and block write transactions.
| COMMAND | MFR_MODEL | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | Block R/W, 2 bytes | |||||||||||||||
| Default # | ||||||||||||||||
MFR_REVISION (0x9B)
The MFR_REVISION command is used to either set or read the manufacturer’s revision number. The actual data for this command is 1 byte. The high order byte here is the byte count in the SMBus block read and block write transactions.
| COMMAND | MFR_REVISION | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | Block R, 2 bytes | |||||||||||||||
| Default # | ||||||||||||||||
IC_DEVICE_ID (0xAD)
Th IC_DEVICE_ID command is a read-only block-read command that returns 2 bytes with the unique device-code identifier for the device. The actual data for this command is 1 byte. The high order byte here is the byte count in the SMBus block read and block write transactions.
| COMMAND | IC_DEVICE_ID | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | Block R, 2 bytes | |||||||||||||||
| Default # | ||||||||||||||||
IC_DEVICE_REV (0xAE)
The IC_DEVICE_REV command is used to read the revision of the IC. The actual data for this command is 1 byte. The high order byte here is the byte count in the SMBus block read and block write transactions.
| COMMAND | IC_DEVICE_ID | |||||||||||||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Access | Block R, 2 bytes | |||||||||||||||
| Default # | ||||||||||||||||