Adding a Software Component
1.
In an
Atmel START
project, select
DASHBOARD
and click on
ADD SOFTWARE COMPONENT
:
2.
Add a USART driver by typing
USART
in the "Filter" field, then add it to your project by clicking the plus sign, or by double-clicking on the line.
Tip:
You can also look for it in the Drivers list.
You will have it displayed in the SELECTED COMPONENTS view:
3.
You can now complete the addition of the USART driver by clicking on the
Add component(s)
button.
The USART driver is added to the application.
Parent topic:
How to Add and Configure Software Components