The following steps describe how to use the output from Atmel START in Atmel Studio.
A new Atmel Studio project will be created, and the files will be imported.
Some projects contain documentation formatted for Doxygen.
Start can be opened in a window inside Studio to generate a project or load an example project.
Settings are accessed from menu
.A backup of the project is taken when reconfiguring with Atmel START. Backups are stored in the folder ‘.atmel-start-backup’ under the project folder.