When your project is configured in Atmel START, you must export it in order to use it in a C compiler.
Atmel Studio
The following steps describe how to use the output from Atmel START in Atmel Studio.
IAR Embedded Workbench
The following steps describe how to use the output from Atmel START in IAR Embedded Workbench. Make sure you have the latest updates of IAR Embedded Workbench installed.
Keil µVision
The following steps describe how to use the output from Atmel START in Keil µVision.
GNU C Makefile
The output from Atmel START can be used with GNU C using a Makefile.
SOMNIUM DRT
The following steps describe how to use the output from Atmel START in SOMNIUM DRT.