SOMNIUM DRT
The following steps describe how to use the output from Atmel START in SOMNIUM DRT.
Exporting the Project from Atmel
START
- 1.
On the Atmel START website, create a new
project (Example or Board).
- 2.
Click on the Export Software Component button. For
exporting project for Atmel Studio and Somonium IDE, select Atmel
Studio.
- 3.
Click on DOWNLOAD PACK.
An ‘atmelstart.atzip’ pack file
will be downloaded.
Steps to Import Atmel START Output into SOMNIUM DRT
- 1.
Launch SOMNIUM DRT.
- 2.
Select to open the import dialog.
- 3.
In the General folder select Existing Projects into Workspace and click
Next.
- 4.
Choose the Select Archive File radio button and
browse to the ‘.atzip’ file exported from Atmel
START.
- 5.
Click Next, then Finish, and a new DRT project
will be created in the workspace with the imported files.