MPLAB™ X IDE
Creating an MPLAB
X Project
- 1.
On the Atmel START website (start.atmel.com/), create a new project (Example or
Board).
- 2.
Once the project is created, go to the EXPORT
PROJECT page and check the "MPLAB X IDE" box.
Importing Atmel Start Project in MPLAB X
- 1.
Select as shown below:
- 2.
Browse the ‘.atzip’ file, as shown below:
- 3.
Follow the procedures described in the wizard.
- 4.
An MPLAB X project will get created.