Control C

Name:
CTRLC
Offset:
0x02
Reset:
0x00
Access:
-
Bit76543210
CMPDSELCMPCSELFIFTYAUPDATECMPOVR
AccessR/WR/WR/WR/WR/W
Reset00000

Bit 7 – CMPDSEL: Compare D Output Select

Compare D Output Select

This bit selects which waveform will be connected to output D.

ValueNameDescription
0 PWMA Waveform A
1 PWMB Waveform B

Bit 6 – CMPCSEL: Compare C Output Select

Compare C Output Select

This bit selects which waveform will be connected to output C.

ValueNameDescription
0 PWMA Waveform A
1 PWMB Waveform B

Bit 3 – FIFTY: Fifty Percent Waveform

Fifty Percent Waveform

If the two waveforms have identical characteristics, this bit can be written to ‘1’. This will cause any values written to the TCDn.CMPBSET/TCDn.CLR register to also be written to the TCDn.CMPASET/TCDn.CLR register.

Bit 1 – AUPDATE: Automatically Update

Automatically Update

If this bit is written to ‘1’, synchronization at the end of the TCD cycle is automatically requested after the Compare B Clear High (TCDn.CMPBCLRH) register is written.

If the fifty percent waveform is enabled by setting the FIFTY bit in this register, writing the Compare A Clear High register will also request a synchronization at the end of the TCD cycle if the AUPDATE bit is set.

Bit 0 – CMPOVR: Compare Output Value Override

Compare Output Value Override

When this bit is written to ‘1’, default values of the Waveform Outputs A and B are overridden by the values written in the Compare x Value in Active state bit fields in the Control D register. See the CTRLD register description for more details.