4.4.2 RISC-V Flash Image Setting

As shown in the following figure, add the --change-section-lma *-0x80000000 command to remove the non-linear address (the first line) of the HEX file.

Figure 4-13. RISC-V Flash Image Setting