26.4.8.4.2 TRIG Negation When PTGTOGL =
1
If generating an individual trigger output when the PTGTOGL bit (PTGCON[12]) =
1, the TRIG outputs will remain set until the
PTGTRIG command is executed again. On the start of the
PTGTRIG command execution, the TRIG outputs are toggled at the
beginning of the PTG execution clock.
Note: The PTGTOGL bit has no effect on the operation of the
‘
PTGCTRL 0b1111’ multiple trigger (broadcast) generation command
with the following exception:- If a target trigger output is
already in the logic ‘
1’ state, having been triggered individually while PTGTOGL is active, the ‘PTGCTRL 0b1111’ command will have no effect and the trigger output will remain at logic ‘1’.