11.6 Crystal Oscillator

The table below provides the crystal oscillator characteristics.

Table 11-8. 24 MHz Crystal Oscillator Characteristics
ParameterTest ConditionSymbolRatingUnit
Min.Typ.Max.
Crystal Oscillator frequencyFundamentalXtal24MHz
Internal parasitic capacitanceBetween XIN and XOUTCPARA24M0.60.70.8pF
Start-up timetON——1ms
Drive levelPON——400µW
Load capacitanceCLOAD4—18pF
Important: Locate the crystal as close as possible to the XOUT and XIN pins.

The following figure shows the crystal oscillator schematic.

Figure 11-1. 24 MHz Crystal Oscillator Schematic
CX = 2 x (CXTAL – CPARA24M – CPCB /2)

Where:

  • CXTAL is the load capacitance of the crystal.
  • CPARA24M is the internal parasitic impedance of the oscillator, typically 0.7 pF.
  • CPCB is the ground-referenced parasitic capacitance of the printed circuit board (PCB) on the XIN and XOUT tracks.

Table 11-9 summarizes recommendations to be followed when choosing a crystal.

The PLC protocol firmwares support propagation of the input clock signal through the TXRX1 pin, allowing fine adjustment of the Cx parameter.

The drive level indicates power consumption by the crystal unit while the oscillation circuit works. Excessive drive level might cause unexpected change of frequency, crystal damage, or shorter device lifetime. The drive level is given by the following formula:

Drive Level=ESR×I2

Where:
  • ESR is the equivalent series resistor (specified by the crystal manufacturer).
  • I is the current flowing through the crystal in RMS. If the waveform is sine wave or similar, the effective value is calculated by Ip-p/2√2.

To keep the drive level value inside the manufacturer range, it is required to limit the current that flows through the crystal. The total power dissipated by the crystal is proportional to RS (see Figure 11-1), therefore its value can be modified to obtain a drive level that complies with the requirements. As the value of RS relates to the safety factor, there is a maximum value of RS that maintains a good safety factor and at the same time keeps the drive level below the crystal manufacturer maximum specifications.

Table 11-9. Recommended Crystal Characteristics
ParameterSymbolRatingUnit
Min.Typ.Max.
Equivalent Series ResistorESR——100Ω
Motional capacitanceCM2—3.2fF
Shunt capacitanceCSHUNT——1.3pF
Frequency tolerance——10(1)25ppm
Notes:
  1. As required by the G3-PLC specification, the system clock tolerance must not exceed ±25 ppm. For the PRIME specification, the maximum allowable tolerance is ±50 ppm, while for the Meters and More specification, it is ±150 ppm. Regardless of the specification, Microchip recommends selecting a crystal with a frequency tolerance that is lower than the specified maximum. This is due to actual performance may be affected by production tolerances, temperature stability, and aging.