3.1.9 mcAppI_OverCurrentReactionIsr
C
/* Over current reaction ISR */
void mcAppI_OverCurrentReactionIsr( uint32_t status, uintptr_t context );
Summary
Overcurrent Reaction Interrupt Service Routine (ISR).
Description
This function is intended to be called when an over current condition is detected in a motor control system. Upon triggering the interrupt, this function will execute to handle the event by taking appropriate actions such as resetting the motor control application,disable the PWM, and triggering the fault indication.
Precondition
The function to be called must be set using mcHalI_PwmCallbackRegister().
Parameters
| Param | Description |
|---|---|
| status | Interrupt status. |
| context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None
Example
void mcAppI_OverCurrentReactionIsr( uint32_t status, uintptr_t context )
{
}
mcHalI_PwmCallbackRegister( (PWM_CALLBACK)mcAppI_OverCurrentReactionIsr, (uintptr_t)dummyForMisra );
Remarks
None.