3.8.5 DHCP Relay Configuration
Configure the DHCP relay agent that is used to forward and transfer DHCP messages between the clients and the server when they are not in the same subnet domain.
Command Syntax:
ip dhcp relay
ip helper-address <v_ipv4_ucast>
ip dhcp relay information option
ip dhcp relay information policy { drop | keep | replace }Argument | Description | |
Parameter |
| IP address of the DHCP relay server |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Enable and configure the DHCP relay server. To disable the DHCP relay server, use the ‘no’ form of the command. | |
Example | Example 1: Enable the DHCP relay server and drop the package when a DHCP message that already contains relay information is received. | |