3.11.3 LACP System Configuration
Use this command to specify if the group performs automatic link (re-)calculation when links with higher priority become available (revertive) and the maximum number of active bundled LACP ports allowed in an aggregation. Also, set the LACP timeout on the port, that is, how fast to transmit BPDUs, once a sec (fast) or once each 30 sec (slow) and the priority.
Command Syntax:
lacp failover { revertive | non-revertive }
lacp max-bundle <v_uint>
lacp timeout { fast | slow }
lacp port-priority <v_1_to_65535>
lacp system-priority <v_1_to_65535>Argument | Description | |
Parameter |
| Group performs automatic link (re-)calculation |
| Group will not perform automatic link (re-)calculation | |
| This parameter only applies to LACP-enabled groups. It determines the maximum number of active bundled LACP ports allowed in an aggregation. | |
| Priority value 1 to 65535, lower means higher priority. | |
Default | Revertive failover is enabled. | |
Mode | LLAG mode and Port List Interface mode | |
Usage | Specify if the group performs automatic link (re-)calculation. To revert to default, use the ‘no’ version of the command. | |
Example | Example 1: Set failover to non-revertive on interface LLAG 1 with max bundle 4. | |