For the ADC to meet its specified accuracy, the charge holding capacitor (CHOLD)
must be allowed to fully charge to the input channel voltage level. The Analog Input model
is shown in the following figure. The source impedance (RS) and the internal
sampling switch (RSS) impedance directly affect the time required to charge the
capacitor CHOLD. The sampling switch (RSS) impedance varies over the
device voltage (VDD). Refer to the following figure.
Figure 32-4. Analog Input Model
Note:
Refer to the “I/O Ports”
section in the “Electrical Specification” chapter.
Important:The
maximum recommended impedance for analog sources is 10 kΩ.
If the source
impedance is decreased, the acquisition time may be decreased. After the analog input
channel is selected (or changed), an ADC acquisition must be completed before the
conversion can be started. To calculate the minimum acquisition time, the following
equation may be used. This equation assumes that 1/2 LSb error is used (4,096 steps for the
ADC). The 1/2 LSb error is the maximum error allowed for the ADC to meet its specified
resolution.
Equation 32-1. Acquisition Time Example
Assumptions: Temperature = 50°C and external impedance pf 10 kΩ, 5.0V VDD
TACQ = Amplifier Settling Time + Hold Capacitor Charging Time + Temperature
Coefficient
= TAMP + TC + TCOFF
= 2 μs + TC + [(Temperature - 25°C)(0.05 μs/°C)]
The value for TC can be approximated with the following equations:
Note: Where n = number of bits of the ADC.
Solving for TC:
Therefore:
Note:
The reference voltage (VREF) has no effect on the equation, since it
cancels itself out.
The charge holding capacitor (CHOLD) is not discharged after each
conversion.
The maximum recommended impedance for analog sources is 10 kΩ. This is required
to meet the pin leakage specification.