9.20.1.1 +WSTAC
This command is used to read or set the DCE’s Wi-Fi station mode configuration. This command is a configuration command which supports setting and getting parameter values. The behavior of configuration commands is described in general in the Configuration Commands section.
Security – Default Security for the command is: GGGG
|
Command |
Description |
Security |
|---|---|---|
|
|
Query all configuration elements |
|
|
|
Query a single element |
|
|
|
Set a single element |
|
|
Parameter Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Integer String Byte Array |
Parameter value |
|
Response |
Description |
|---|---|
|
|
Read response |
|
Element Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Any |
Parameter value |
|
ID |
Name |
Type |
Description |
Security |
|---|---|---|---|---|
|
1 |
|
String |
Network name Maximum length is 32 |
|
|
2 |
|
Integer |
Security type
|
|
|
3 |
|
String |
Credentials for connecting to the network Maximum length is 128 |
|
|
4 |
|
Integer |
The channel the network must reside on (or 0 for any). Valid range is 0-13 |
|
|
5 |
|
MAC Address |
The BSSID of the network to connect to |
|
|
7 |
|
Integer |
Connection timeout in milliseconds |
|
|
8 |
|
Unsigned Integer |
Network interface index |
|