41.8.18 SDHC Error Interrupt Status Register

Table 41-19. Register Bit Attribute Legend
SymbolDescriptionSymbolDescriptionSymbolDescription
RReadable bitHCCleared by Hardware(Grey cell)Unimplemented
WWritable bitHSSet by HardwareXBit is unknown at Reset
KWrite to clearSSoftware settable bit——
Name: EISTR
Offset: 0x32
Reset: 0x0000
Property: -

Bit 15141312111098 
    BOOTAE  ADMAACMD 
Access R/WR/WR/W 
Reset 000 
Bit 76543210 
 CURLIMDATENDDATCRCDATTEOCMDIDXCMDENDCMDCRCCMDTEO 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bit 12 – BOOTAE Boot Acknowledge Error

Note: This register entry is specific to the e.MMC operation mode.

This bit is set to 1 when detecting that the e.MMC Boot Acknowledge Status has a value other than “010”.

This bit can only be set to 1 if SDHC_EISTER.BOOTAE is set to 1. An interrupt can only be generated if SDHC_EISIER.BOOTAE is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 9 – ADMA ADMA Error

This bit is set to 1 when the peripheral detects errors during an ADMA-based data transfer. The state of the ADMA at an error occurrence is saved in SDHC_AESR.

In addition, the peripheral rises this status bit when it detects some invalid description data (Valid=0) at the ST_FDS state (refer to section “Advanced DMA” in the “SD Host Controller Simplified Specification V3.00”. ADMA Error Status (ERRST) in SDHC_AESR indicates that an error occurs in ST_FDS state. The user may find that the Valid bit is not set at the error descriptor.

This bit can only be set to 1 if SDHC_EISTER.ADMA is set to 1. An interrupt can only be generated if SDHC_EISIER.ADMA is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 8 – ACMD Auto CMD Error

Auto CMD12 and Auto CMD23 use this error status. This bit is set to 1 when detecting that one of the 0 to 4 bits in SDHC_AESR (SDHC_ACESR[4:0]) has changed from 0 to 1. In the case of Auto CMD12, this bit is set to 1, not only when errors occur in Auto CMD12, but also when Auto CMD12 is not executed due to the previous command error.

This bit can only be set to 1 if SDHC_EISTER.ACMD is set to 1. An interrupt can only be generated if SDHC_EISIER.ACMD is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 7 – CURLIM Current Limit Error

By setting SD Bus Power (SDBPWR) in SDHC_PCR, the peripheral is requested to supply power for the SD Bus. The peripheral is protected from an illegal card by stopping power supply to the card, in which case this bit indicates a failure status. Reading 1 means the peripheral is not supplying power to the card due to some failure. Reading 0 means that the peripheral is supplying power and no error has occurred. The peripheral may require some sampling time to detect the current limit.

This bit can only be set to 1 if SDHC_EISTER.CURLIM is set to 1. An interrupt can only be generated if SDHC_EISIER.CURLIM is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 6 – DATEND Data End Bit Error

This bit is set to 1 either when detecting 0 at the end bit position of read data which uses the DAT line or at the end bit position of the CRC Status.

This bit can only be set to 1 if SDHC_EISTER.DATEND is set to 1. An interrupt can only be generated if SDHC_EISIER.DATEND is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 5 – DATCRC Data CRC Error

This bit is set to 1 when detecting a CRC error during a transfer of read data which uses the DAT line or when detecting that the Write CRC Status has a value other than '010'.

This bit can only be set to 1 if SDHC_EISTER. DATCRC is set to 1. An interrupt can only be generated if SDHC_EISIER. DATCRC is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 4 – DATTEO Data Timeout error

This bit is set to 1 when detecting one of following timeout conditions:
  • Busy timeout for R1b, R5b response type (see “Physical Layer Simplified Specification V3.01” and “SDIO Simplified Specification V3.00” ).
  • Busy timeout after Write CRC Status.
  • Write CRC Status timeout.
  • Read data timeout.

This bit can only be set to 1 if SDHC_EISTER.DATTEO is set to 1. An interrupt can only be generated if SDHC_EISIER.DATTEO is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 3 – CMDIDX Command Index Error

This bit is set to 1 if a Command Index error occurs in the command response.

This bit can only be set to 1 if SDHC_EISTER.CMDIDX is set to 1. An interrupt can only be generated if SDHC_EISIER.CMDIDX is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 2 – CMDEND Command End Bit Error

This bit is set to 1 when detecting that the end bit of a command response is 0.

This bit can only be set to 1 if SDHC_EISTER.CMDEND is set to 1. An interrupt can only be generated if SDHC_EISIER.CMDEND is set to 1.

Writing this bit to 1 clears this bit.

ValueDescription
0

No error

1

Error

Bit 1 – CMDCRC Command CRC Error

The Command CRC Error is generated in two cases.

If a response is returned and Command Timeout Error (CMDTEO) is set to 0 (indicating no command timeout), this bit is set to 1 when detecting a CRC error in the command response.

The peripheral detects a CMD line conflict by monitoring the CMD line when a command is issued. If the peripheral drives the CMD line to 1 level, but detects 0 level on the CMD line at the next SDCLK edge, then the peripheral aborts the command (stops driving the CMD line) and sets this bit to 1. CMDTEO is also set to 1 to indicate a CMD line conflict.

This bit can only be set to 1 if SDHC_EISTER.CMDCRC is set to 1. An interrupt can only be generated if SDHC_EISIER.CMDCRC is set to 1.

Writing this bit to 1 clears this bit.

Bit 0 – CMDTEO Command Timeout Error

This bit is set to 1 only if no response is returned within 64 SDCLK cycles from the end bit of the command. If the peripheral detects a CMD line conflict, in which case Command CRC Error (CMDCRC) is also set to 1, this bit is set without waiting for 64 SDCLK cycles because the command is aborted by the peripheral.

This bit can only be set to 1 if SDHC_EISTER.CMDTEO is set to 1. An interrupt can only be generated if SDHC_EISIER.CMDTEO is set to 1.

Writing this bit to 1 clears this bit.

Table 41-20. CMD Error Types
CMDCRCCMDTEOTypes of error
00No error
01Response timeout error
10Response CRC error
11CMD line conflict