The Trap Configuration provides SNMP trap source configurations. A Trap Destination Address is sent for the given trap source, if at least one filter matches with the included filter type. The following figure shows the SNMP trap source configuration.Figure 4-5. SNMP-Trap Source Configuration
The trap source configuration page has the following parameters:
Name: The event for which a trap must be sent. See the preceding figure.
Type: Include/exclude trap for the specified event
Subset OID: The subset OID for the entry. The value must depend on the kind of trap that is sent. For example, the ifIdex is the subset OID of linkUp and linkDown. A valid subset OID is one or more digital numbers (0–4294967295) or asterisk (*) which are separated by dots (.). The first character must not begin with asterisk (*) and the maximum OID count must not exceed 128.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.