4.27.8 QoS DSCP Translation Configuration
The DSCP Translation page allows you to configure the basic QoS DSCP Translation settings for all switches. DSCP translation can be done in Ingress or Egress.

The DSCP Translation page has the following parameters:
- DSCP: Maximum number of supported DSCP values are 64 and valid DSCP value ranges 0-63
- Ingress: Ingress side DSCP can be first translated to new DSCP before using the DSCP for CoS and DPL map. There are two configuration parameters for DSCP Translation:
- Translate: DSCP at Ingress side can be translated to any of (0–63) DSCP values
- Classify: Click to enable Classification at Ingress side
- Egress: There are the following configurable parameters for Egress side:
- Remap DP0: Controls the remapping for frames with DP level 0. Select the DSCP value from the Select menu to which you want to remap. DSCP value ranges from 0–63.
- Remap DP1: Controls the remapping for frames with DP level 1. Select the DSCP value from the Select menu to which you want to remap. DSCP value ranges from 0–63.