The QoS Control List Configuration page shows the QoS Control List (QCL), which is made up of the QCEs. Each row describes a QCE that is defined. The maximum number of QCEs is 256 on each switch.
Click the plus icon to add a new QCE to the list.Figure 4-105. QoS Control List
Configuration
Figure 4-106. QCE ConfigurationThe QoS Control List Configuration page has the following
parameters:
QCE: Indicates the QCE id
Port: Indicates the list of ports configured with the QCE or Any
DMAC: Indicates the destination MAC address. Possible values are:
Any: Match any DMAC
Unicast: Match unicast DMAC
Multicast: Match multicast DMAC
Broadcast: Match broadcast DMAC
<MAC>: Match
specific DMAC
SMAC: Match specific source MAC address or Any
Tag Type: Indicates tag type. Possible values are:
Any: Match tagged and untagged frames
Untagged: Match untagged frames
Tagged: Match tagged frames
C-Tagged: Match C-tagged frames
S-Tagged: Match S-tagged frames
VID: Indicates (VLAN ID), either a specific VID or range of VIDs. VID can be in the range of 1–4095 or Any.
PCP: Priority Code Point. Valid values of PCP are specific (0, 1, 2, 3, 4, 5, 6, and 7) or range (0–1, 2–3, 4–5, 6–7, 0–3, and 4–7) or Any.
DEI: Drop Eligible Indicator. Valid value of DEI is 0, 1 or Any.
Frame Type: Indicates the type of frame. Possible values are:
Any: Match any frame type
Ethernet: Match EtherType frames
LLC: Match (LLC) frames
SNAP: Match (SNAP) frames
IPv4: Match IPv4 frames
IPv6: Match IPv6 frames
Action: Indicates the classification action taken on ingress frame if the configured parameters are matched with the frame's content. The following are the possible actions: