The interaction and command sequence are the same with serial DFU except for the extra parameters in the Enter DFU Mode command and the response of the DFU Update Request command. In the OTAPC-based device update method, before initiating the DFU command, it is mandatory to have a successful and secure Bluetooth Low Energy connection between two RNBD451 devices. As the OTAPC is an OTA update to a remote device, the DFU update request command sends an OTA request to the remote device for approval. Upon accepting the request, the firmware distribution is initiated.
The following figure illustrates a sample MSC for DFU to remote peer over OTAPC. Figure 5-28. Sample MSC for RNBD451 OTA using Remote Peer Over OTAPCFollowing are the commands used on the OTA Client side. The OTAPC tool is used to send these commands to the OTA client.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.