5.3.4.1 Set Central Initial Connection Parameter (ST,<hex16>…)
Format: ST,<hex16>,<hex16>,<hex16>,<hex16>
This command sets the initial connection parameters of the central device for future connections. This command expects four input parameters, and all are 16-bit values in hex format. For any modifications in current connection parameters, refer to Request Connection Parameter Update (T,<hex16>…).
The corresponding get command, GT, returns the desirable connection parameters set by command ST when the connection is not established. When the connection is established, the actual connection parameters display in response to command GT.
Connection interval, latency and timeout are often associated with how frequently a peripheral device must communicate with the central device and are , therefore, closely related to power consumption. The following table provides details about the parameters, range and description.
The connection parameters need to adhere to the following rules.
Latency <= 30
Parameter | Range | Description |
|---|---|---|
Minimum interval | 0x0006-0x0C80 |
|
Maximum interval | 0x0006-0x0C80 |
|
Latency | 0x0000-0x01F3 Must be less than ((Timeout*10/Inter- val*1.25)-1) | The maximum number of consecutive connection events. The peripheral device is not required to communicate with the central device. |
Timeout | 0x000A-0x0C80 |
|
| Default: | 0010, 0010, 0000, 0048 | |
| Example: | ST,0020,0064,0002,0064 | // Set the interval between 40-125 ms, latency to 2 events and timeout to 1s |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter | |
Note: The PDS stores these parameters. The parameters are effective immediately. Apple® iOS® devices have some special requirements for these parameters. The connection parameter update may be rejected if it does not comply with the rules. For more information, refer to the Accessory Design Guidelines on the Apple developer website. | ||