5.3.4.5 Connect Specific Bonded Device (C<1-8>)
Format:
C<1-8>
The RNBD451 module can store the MAC addresses
for up to eight bonded devices. The C command provides an easy way to
reconnect to any stored device without typing the MAC address of the stored device, if
the device uses a public address. When this command is used to reconnect to a bonded
device, the RNBD451 module automatically secures
the link when the connection is established. To display the list of stored devices, use
command LB.
| Example: | C2 | // Reconnect to the second stored device |
| Response: | Trying
| // Start connecting |
%CONNECT% | // Status string | |
Err | // Syntax error or invalid parameter | |
%ERR_CONN% | // Status string |