5.3.4.8 Set PHY Preference (CSPHY,<hex16>…)
Format: CSPHY,<hex16>,<hex8>,<hex8>,<hex8>
Use this command to set the PHY preferences for the specified connection. The CSPHY command expects four input parameters. The first parameter is a 16-bit hex value that indicates which connection handle corresponds to a specific Bluetooth Low Energy connection. The second parameter is an 8-bit bitmap defined in Table 5-19 that sets the preferred PHY’s transmitter. The third parameter is an 8-bit bitmap to set the preferred PHY's receiver. For the value definition, refer to Table 5-19. The last is the PHY option, which is used when the coded PHY is selected and defined in Table 5-20.
| PHY’s Bitmap (HEX) | Description |
|---|---|
| 00 | No preferred |
| 01 | 1M PHY |
| 02 | 2M PHY |
| 04 | Coded PHY |
| PHY’s Option (HEX) | Description |
|---|---|
| 00 | No preferred |
| 01 | S2 coded PHY |
| 02 | S8 coded PHY |
| Example: | CSPHY,0071,03,03,00 | // Set the preferred PHY of TX and RX to 1M/2M PHY in the Bluetooth® Low Energy link for connection handle 0x0071 |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter | |
%PHY_UPDATED,<ConnHandle>,<Tx PHY>,<Rx PHY>% | // PHY update success status report | |
%ERR_PHYUPDATE,<ConnHandle>% | // PHY update fail status report | |
Note:
| ||