5.5.11 Set PMU Mode (SPMU,<0,1>)
Format: SPMU,<0,1>
This command is used to set the PMU mode as MLDO mode or BUCK PWM mode. There is one parameter, which is ‘
0’ or ‘1’.- ‘
0’ – To select MLDO mode - ‘
1’ – To select BUCK PWM mode
| Default: | 0 | |
| Example: | SPMU,1 | // Set PMU mode as the BUCK PWM mode |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter | |
Note: The PDS stores this parameter. The parameter is effective after a reboot. | ||