1.2.3.19 SYS_MQTT_Subscribe Function
C
int32_t SYS_MQTT_Subscribe(SYS_MODULE_OBJ obj,
SYS_MQTT_SubscribeConfig *subConfig);Summary
Returns success/ failure for the subscribing to a Topic by the user.
Description
This function is used for subscribing to a Topic.
Precondition
SYS_MQTT_Connect should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| obj | SYS MQTT object handle, returned from SYS_MQTT_Connect subConfig - valid pointer to the Topic details on which to Subscribe |
Returns
SYS_MQTT_SUCCESS - Indicates that the Request was catered to successfully
SYS_MQTT_FAILURE - Indicates that the Request failed
Example
SYS_MQTT_SubscribeConfig sSubscribeCfg; memset(&sSubscribeCfg, 0, sizeof(sSubscribeCfg)); sSubscribeCfg.qos = 1; strcpy(sSubscribeCfg.topicName, "house/temperature/first_floor/kitchen"); // Handle "objSysMqtt" value must have been returned from SYS_MQTT_Connect. if( SYS_MQTT_Subscribe(objSysMqtt, &sSubscribeCfg) == SYS_MQTT_SUCCESS) { }