1.2.3.20 SYS_MQTT_Unsubscribe Function
C
int32_t SYS_MQTT_Unsubscribe(SYS_MODULE_OBJ obj, char *subTopic);Summary
Returns success/ failure for the unsubscribing to a Topic by the user.
Description
This function is used for Unsubscribing from a Topic.
Precondition
SYS_MQTT_Connect should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| obj | SYS MQTT object handle, returned from SYS_MQTT_Connect subtopic - Topic from which to unsubscribe |
Returns
SYS_MQTT_SUCCESS - Indicates that the Request was catered to successfully
SYS_MQTT_FAILURE - Indicates that the Request failed
Example
// Handle "objSysMqtt" value must have been returned from SYS_MQTT_Connect.
if( SYS_MQTT_Unsubscribe(objSysMqtt, "house/temperature/first_floor/kitchen") == SYS_MQTT_SUCCESS)
{
}