13.6.3.3.2 Function port_pin_get_output_level()
Retrieves the state of a port pin that is configured as an output.
bool port_pin_get_output_level( const uint8_t gpio_pin)
Reads the current logical output level of a port pin and returns the current level as a Boolean value.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
gpio_pin |
Index of the GPIO pin to read |
Returns
Status of the port pin's output buffer.