13.6.3.3.3 Function port_pin_set_output_level()
Sets the state of a port pin that is configured as an output.
void port_pin_set_output_level( const uint8_t gpio_pin, const bool level)
Sets the current output level of a port pin to a given logic level.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | gpio_pin |
Index of the GPIO pin to write to |
[in] | level |
Logical level to set the given pin to |