25.8.7 Quick Start Guide for Using DMA with TCC
SAM D21/R21/L21/L22/DA1/C21 Xplained Pro
In this use case, the TCC will be used to generate a PWM signal. Here the pulse width varies through following values with the help of DMA transfer: one quarter of the period, half of the period, and three quarters of the period. The PWM output can be used to drive an LED. The waveform can also be viewed using an oscilloscope. The output signal is also fed back to another TCC channel by event system, the event stamps are captured and transferred to a buffer by DMA.
Board | Pin | Connect to |
|---|---|---|
SAMD21 Xpro | PB30 | LED0 |
SAMR21 Xpro | PA19 | LED0 |
SAML21 Xpro | PB10 | LED0 |
SAML22 Xpro | PC27 | LED0 |
SAMDA1 Xpro | PB30 | LED0 |
SAMC21 Xpro | PA15 | LED0 |
GCLK generator 0 (GCLK main) clock source
Use double buffering write when set top, compare, or pattern through API
No dithering on the counter or compare
Prescaler is set to 1024
Single Slope PWM wave generation
GCLK reload action
Don't run in standby
No fault or waveform extensions
No inversion of waveform output
No capture enabled
Count upward
Don't perform one-shot operations
Counter starts on 0
Counter top set to 0x1000
Channel 0 (on SAM D21 Xpro) or 3 (on SAM R21 Xpro) is set to compare and match value 0x1000*3/4 and generate event
Channel 1 is set to capture on input event
TCC match capture channel 0 (on SAM D21 Xpro) or 3 (on SAM R21 Xpro) is selected as event generator
Event generation is synchronous, with rising edge detected
TCC match capture channel 1 is the event user
Two DMA resources are used
Both DMA resources use peripheral trigger
Both DMA resources perform beat transfer on trigger
Both DMA resources use beat size of 16 bits
Both DMA resources are configured to transfer three beats and then repeat again in same buffer
- On DMA resource which controls the compare value
TCC0 overflow triggers DMA transfer
The source address increment is enabled
The destination address is fixed to TCC channel 0 Compare/Capture register
- On DMA resource which reads the captured value
TCC0 capture on channel 1 triggers DMA transfer
The source address is fixed to TCC channel 1 Compare/Capture register
The destination address increment is enabled
The captured value is transferred to an array in SRAM