23.6.3.1.2 Function system_pinmux_pin_set_config()
Writes a Port pin configuration to the hardware module.
void system_pinmux_pin_set_config( const uint8_t gpio_pin, const struct system_pinmux_config *const config)
Writes out a given configuration of a Port pin configuration to the hardware module.
Note: If the pin direction is set as an output, the pull-up/pull-down input configuration setting is ignored.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | gpio_pin |
Index of the GPIO pin to configure |
[in] | config |
Configuration settings for the pin |