7.6.4.2 Function dma_add_descriptor()
Add a DMA transfer descriptor to a DMA resource.
enum status_code dma_add_descriptor( struct dma_resource * resource, DmacDescriptor * descriptor)
This function will add a DMA transfer descriptor to a DMA resource. If there was a transfer descriptor already allocated to the DMA resource, the descriptor will be linked to the next descriptor address.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | resource |
Pointer to the DMA resource |
[in] | descriptor |
Pointer to the transfer descriptor |
| Return value | Description |
|---|---|
STATUS_OK |
The descriptor is added to the DMA resource |
STATUS_BUSY |
The DMA resource was busy and the descriptor is not added |