4.1 Installing PCIe Demo Application
(Ask a Question)To install the PolarFire PCIe Demo application, perform the following steps:
- Install the GUI (setup.exe) from the following design files folder: mpf_an4597_df\GUI
- Double click the
setup.exein the provided GUI installation:(GUI\setup.exe).
- Apply default options, as shown in the following figure.
Figure 4-1. Installing PCIe Demo Application 
- To start the installation, click Next.
- To complete the installation, click Finish.
Figure 4-2. Successful Installation of PCIe Demo Application