1.9.1.12 ADC_CoreInterruptsStatusClear Function
C
void ADC_CoreInterruptsStatusClear(ADC_CORE_NUM core, ADC_CORE_INT interruptMask)
Summary
Clears the specified ADC core's interrupt status
Description
This function clears the requested interrupt status bits of the specified ADC core
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
core | ADC core n Mask of ADC core interrupts to clear status. Bitwise OR of the following macros: ADC_CORE_INT_CHRDY_0 ADC_CORE_INT_CHRDY_1 ADC_CORE_INT_CHRDY_2 ADC_CORE_INT_CHRDY_3 ADC_CORE_INT_CHRDY_4 ADC_CORE_INT_CHRDY_5 ADC_CORE_INT_CHRDY_6 ADC_CORE_INT_CHRDY_7 ADC_CORE_INT_EOSRDY ADC_CORE_INT_CHNERRC ADC_CORE_INT_FLTRDY ADC_CORE_INT_CHRDYC ADC_CORE_INT_SOVFL ADC_CORE_INT_CMPHIT |
Returns
None
Example
ADC_CoreInterruptsStatusClear(ADC_CORE_NUM1, ADC_CORE_INT_EOSRDY);
Remarks
None