1.9.1.18 ADC_SyncTriggerCounterSet Function
C
void ADC_SyncTriggerCounterSet(uint16_t counterVal)
Summary
Configures the value of CTRLC.CNT register
Description
The Synchronous Trigger (STRIG) is driven by a counter at the ADC Control Clock (CTL_CLK) frequency and fires when the counter reaches the value defined by CTRLC.CNT[7:0]. Use this API to set the value of CTRLC.CNT register.
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
counterVal | value of the CTRLC.CNT |
Returns
None
Example
ADC_SyncTriggerCounterSet(0x300);
Remarks
None