1.9.1.20 ADC_ChannelSamplingStart Function

C

ADC_ChannelSamplingStart(void)

Summary

Enables the Analog Mux Input and starts sampling on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API

Description

Enables the Analog Mux Input and starts sampling. This API must be used in conjuction with ADC_SoftwareControlledConversionEnable() API to start the conversion on the given channel.

Precondition

ADCx_Initialize() function must have been called first for the associated instance.

Parameters

None

Returns

None

Example

ADC_ChannelSamplingStart();

Remarks

None