1.28.10.15 MCANx_ErrorCountGet Function

C

void MCANx_ErrorCountGet(uint8_t *txErrorCount, uint8_t *rxErrorCount) // x - Instance of the MCAN peripheral

Summary

Returns the transmit and receive error count during transfer.

Precondition

MCANx_Initialize must have been called for the associated MCAN instance.

Parameters

Param Description
txErrorCount Transmit Error Count to be received
rxErrorCount Receive Error Count to be received

Returns

None.

Example

uint8_t txErrorCount = 0;
uint8_t rxErrorCount = 0;
MCAN0_ErrorCountGet(&txErrorCount, &rxErrorCount);

Remarks

None.