2.80.20 PDECx_COUNTERCompare0Set Function
C
bool PDECx_COUNTERCompare0Set ( uint16_t compare0 ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Configures Compare 0 register value
Description
This function configures Compare 0 (CC0) register value. This can be period value of the counter if CTRLA.PEREN bit is set.
Precondition
PDECx_COUNTERInitialize function must have been called first for the given channel.
Parameters
| Param | Description |
|---|---|
| compare0 | Value to be set in Compare 0 register |
Returns
true - If Compare 0 register set false - If Compare 0 register is not set
Example
PDEC_COUNTERInitialize();
PDEC_COUNTERStart();
PDEC_COUNTERCompare0Set(0x100);
Remarks
None.