2.80.8 PDECx_QDECStatusGet Function
C
PDEC_QDEC_STATUS PDECx_QDECStatusGet (void) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Identifies status of the quadrature interrupts
Description
This function returns the status of the interrupts that occur in quadrature mode.
Precondition
PDECx_QDECInitialize must have been called first.
Parameters
None
Returns
PDEC_QDEC_STATUS - status of the quadrature interrupts
Example
PDEC_QDEC_STATUS status; status = PDEC_QDECStatusGet();
Remarks
This function is applicable only for quadrature mode.