2.113.25 PMERRLOC_CALLBACK Typedef
C
typedef void (* PMERRLOC_CALLBACK)( uintptr_t context, uint32_t interruptStatus )
Summary
Defines the data type and function signature for the PMERRLOC peripheral callback function.
Description
This data type defines the function signature for the PMERRLOC peripheral callback function. The PMERRLOC peripheral will call back the client's function with this signature when the PMERRLOC interrupt has occurred.
Precondition
PMERRLOC_Initialize must have been called for the given PMERRLOC peripheral instance. Callback must have been registered using PMERRLOC_CallbackRegister().
Parameters
| Param | Description |
|---|---|
| context | Allows the caller to provide a context value (usually a pointerto the callers context for multiple clients) |
| interruptStatus | PMERRLOC interrupt status |
Returns
None.
Example
void pmerrlocCallback( uintptr_t context, uint32_t interruptStatus )
{
}
PMERRLOC_CallbackRegister(pmerrlocCallback, (uintptr_t)NULL);
Remarks
None.